Hi Team,
Customer now use TPS62290TDRVRQ1 in their design to output 1.8V to power flash but found 5pcs abnormal when testing 40 pcs.
The abnormal is output change from 1.8V to 1.89V; SW impedance to GND change from 10M ohm to 60ohm.
One thing would like to check with you is when 62990 is power-off, customer will add 1.8V to 62990 output directly. Because customer would like to program flash during the test. And then, 1.8V is removed, customer only use 62990 output to power flash.
May I ask whether it will damage 62290 when adding 1.8V to its output though 62290 doesn't power-up?
And whether customer SCH is ok? Any advice?
Here is abnormal one which is 1.87-1.89V output and come into protection because the temp is high.