Hello,
from 8.5.1 of the data sheet, I can see that overvoltage will be indicated , but what else will happen?
The following I tried with my evaluation board:
LED string with 43V forward voltage
ILED1=100mA
dimming over PWM
Vin 10VDC-50VDC
The LM3492 didn't get hot or any other problem with the dimming.
Is it possible to use the LM3492 permanently under overvoltage conditions?
The chalange is, that I can not use a buck, because we are working with long cables. So at low current over the cable, we have 48VDC at the Vin but if current increases, we have a 25VDC voltage drop. The LED string can not be changed at the moment.
Regards
Andreas