This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM82813: Timing condition for VIN, EN, and MODE/SYNC input

Guru 19565 points
Part Number: TPSM82813

Is TPSM82813 have timing condition for VIN, EN, MODE/SYNC pin on startup? 

For example;

・EN and MODE/SYNC should supply the after than VIN (or the same timing)

・External clock to MODE/SYNC need to wait EN: High + xx ms

・Or, these timing condition are not required

Best regards,

Satoshi