Hi.
I have configured a power supply circuit using this charging IC for mobile devices.
As one of the evaluations, I was checking the charge control according to fig.20, but there were some points that I did not get it.
- When the TS voltage reached vcold state.2, the charging current stopped but the LED remained on. Is this correct?
- When I returned to the Vcool state.3, charging resumed, but the charging current did not reach the target value. Moreover, the LED was turned off. Why is this?
- Once the hardware was reset, it returned to the intended operation state.4. Does it mean that a hard reset is required to return from the Cold Fault to state.4?
I would be grateful if you could give me some advice.
best regards.
state.1 Vcool |
state.2 Vcold |
state.3 Vcool |
hard reset |
state.4 Vcool |
|
LED (nCHG open drain FET) |
ON | ON | OFF | OFF | ON |
BATT charge current |
ON 50% Ichg. |
OFF |
ON but unstable. unless 50% Ichg. |
OFF |
ON 50% Ichg. |