This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54160A: Minimum VIN to transfer VOUT of TPS54160A application

Part Number: TPS54160A

How is relationship between VIN and VOU

for example, i want to design a circuit that  OUTPUT is  6V .

The VIN minimum is 6+(voltage reference 0.8)=6.8V right?

  • Hello, you are interested in the dropout behavior of the device it sounds.

    You can approximate required vin for 6V regulation by:

    6V = Vin - .410*Iout - LDCR*Iout

    LDCR is DCR of output filter inductor.

    I am also considering the Vdrop from power FET at max duty cycle, which is close to 100%. This is an approximation.