This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: LM5069MM-2/NOPB

Part Number: LM5069

These are the following requirements:

  • Maximum Input Voltage = 30V
  • Minimum Input Voltage = 10V
  • Maximum Load Current = 10A
  • Nominal Load Voltage =  24VDC

I would like the LM5069 to have an OVL of 30Vand UVL of 10V. 

I would like the LM5069 to operate in a constant current mode and the Fault Response to be in Retry Mode.

  1. How do I estimate the Maximum Output Load Capacitance: CLOAD
  2. What is the difference between Minimum Power Limit to Ensure Vsns > 5mV (PLIM,MIN) and Target Power Limit?
  3. Is the Target Power Limit more than the maximum power draw of the load?
  4. Are there any TI N-MOSFETs currently in stock that meet the circuit requirements?