Hello Team,
My customer is designing an SMPS application that is a bit different and struggling to find a chip that will work. Low power (about 1 watt), half-bridge, the tiny overall size (10mm).
So they need
-wide input voltage range (3.0v to 36v) negotiable
-internal switches (1-2A) high-side and low-side
-PWM controller,
-adjustable frequency (400KHz-1MHz) negotiable
Desirable features
-soft start
-pulse by pulse current limit
-OV/UV lockout
1) Buck controllers seem likely, but it is not clear if switch current can be positive AND negative (half bridge current is symetrical positive and negative). Will the low side switch SINK current?
2) Is there a half-bridge controller appropriate for 1W power levels?
Regards
Reanan