This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: Stability with moderate load capacitance

Part Number: LM5022

I'm in need of a boost configuration that provides high efficiency and acceptable stability with an input voltage of 42V and and an output voltage of 48V with a maximum load current of about 1.6A with a total load capacitance (other, unmodifiable modules) of between 150uF and 200uF. 

I've worked on this design in Webench, but I need to improve the phase margin of the design with this much load capacitance. Webench reported that the stability optimization feature is not enabled for this part. I selected this part because it is one of the few parts with availability. It has been a long time since I've done bode plots and the like, would anyone be able to lend a hand in determining the optimum compensation network to have robust operation? Thanks in advance.

Regards,

Vinny