Hi,
I am going to use TPS753 (digikey) to power up my custom-designed medical device with 3.3V. My device has a maximum current consumption of 400mA and I am planning to use a 3.7V - 2700mAh - Li-Ion battery to feed the device.
Based on the datasheet of the product (datasheet) Figure 11, there will be ~160mV Dropout Voltage @ +25 C which looks fine to get 3.3V from 3.7V battery.
I was wondering if my predication is true or I should take other parameters into consideration?
Thank you,
Sajjad.