This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS753: Regulating 3.7V battery into 3.3V

Part Number: TPS753

Hi,

I am going to use TPS753 (digikey) to power up my custom-designed medical device with 3.3V. My device has a maximum current consumption of 400mA and I am planning to use a 3.7V - 2700mAh - Li-Ion battery to feed the device.

Based on the datasheet of the product (datasheet) Figure 11, there will be ~160mV Dropout Voltage @ +25 C which looks fine to get 3.3V from 3.7V battery.

I was wondering if my predication is true or I should take other parameters into consideration?

Thank you,

Sajjad.