This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54541: Negative voltage output Monitoring Problem

Part Number: TPS54541

Hi,

We have used the TPS54541 IC for +12V &  -12V generation. It is working.  

But when we probe the -12V regulator for current measurement, the IC output was shorted with Ground. (Just Ammeter connected as per diagram, and powered ON. No output from the IC.)

Input voltage is 24VDC.

The Image as  shown below.

Please let us know, why this problem was occurred?  How we can resolve this problem?

Thanks,

Ganesh C