This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546C23: TPS546C23: Query related to TPS546C20A and TPS546C23 Excel Calculator and Layout Checklist

Part Number: TPS546C23

Hello TI Team,

I am working with TI excel sheet to design 3V3@ 25A output by using TPS546C23

S546C23 Excel Calculator and Layout Checklist

https://www.ti.com/lit/zip/slurb05

The Buck inputs are

Parameter Specification Units
Minimum input voltage 11.4 V
Maximum input voltage 12.6 V
Switching frequency 3.00E+05 Hz
     
Output voltage 1 V
Maximum output continuous current 15 A
     
Maximum operating ambient temperature 85 deg C
Peak-to-peak Input Voltage Ripple 1.00E-01 Vpp
Expected Efficiency 0.85 -
     
Peak-to-Peak Output Voltage Ripple 5.00E-03 Vpp
Peak-to-Peak Output Voltage Overshoot 1.00E-02 Vpp
Load transient Starting current level 1.5 A
Load transient Final current level 9 A

while putting the inputs in TPS546C23 Excel Calculator and Layout Checklist, I am getting design waring of LC resonance frequency. 

Can someone helps to clarify and resolve this problem?

Your quick response in this regard will be highly appreciable?

Regards

Kapil