Part Number: TPS630250
Hello,
My name is Kennedy and I am a student working on a school project. I had a question about the operational capabilities of the TPS630250 converter. I am supplying about 3.72V from a Lithium-Ion battery to the TPS630250RNCR converter designed as shown below to get 3.3V output. I have been able to get 3.3V at one point. However, the voltage is not sustaining itself and is dropping to about 100mV. The converter also may have seemed to short itself out under these conditions, but I have no idea what caused the internal damage. If anyone could take a look into this or provide any insight I would greatly appreciate your help. (Please note pin 10 was a blue wire connection and is not in the original PCB design, but is connected to power on the actual PCB)


Regards,
Kennedy