Dear Sir,
Can you use the tpsm63606 to generate the -15V/2A,using the input 12V?
Regards,
Chai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
Can you use the tpsm63606 to generate the -15V/2A,using the input 12V?
Regards,
Chai
Hi Chai,
Yes the TPSM63606 can be used to convert from buck to inverting buck for a 12Vin|-15Vout|2A application.
For more detail and guidance on this conversion, please refer to the app note (https://www.ti.com/lit/an/snva856a/snva856a.pdf).
Regards,
Jimmy
Can it work? Input 12V , output 15V 2A
If you want a +12VIN to +15VOUT, then you will need to get a boost regulator.
The TPSM63606 is only a buck/ step-down module so it would not be applicable for a +12Vin| +15Vout application.
Correct, this module can be configured as a buck or inverting buck-boost (IBB). See the IBB application example in the datasheet: