Part Number: BQ24103
Hi team,
Here's an issue from the customer may need your help:
The customer is developing a BQ24103-based charger. Input: 10V 2A. IC output current: 2 A.
During the charging process, the surface temperature of the IC rises up to 120°C, is this proper? If not, is there any way to reduce the temperature rise?
Could you help check this case? Thanks.
Best Regards,
Cherry