Hi experts,
My customer want to use TPS54308 in the Flybuck circuit. But He met a error report when he simulated the circuit with PSpice for TI.
Below is the simulation circuit. The parameter is : Input voltage=15V, nos-isolated output voltage Vo=5V Io=0.1A, isolated output voltage1 Vo1=24V Io1=0.1A, isolated output voltage2 Vo2=24V Io2=0.1A.
Could you please help me creat a correct simulation file for verifying the circuit, many thanks!
Thanks and BR,
Gordon