Other Parts Discussed in Thread: TPS40210, LM5176, LM25118, LM317
Hi
I am planning this part LM5118 with input voltage 12V and 1A(max. input current) & Max. output voltage 25V with the current limit of 350mA.
So I want to protect my input power supply by limiting the input current (or) output current by varying the output voltage similar to constant current control driving.
Is it possible to implement these features? Also one more point, In the datasheet One feature mentioned as Emulated Peak Current Mode Control