Other Parts Discussed in Thread: LM5019, LM5164, LM5163
Dear TI expert,
Application Description
1) 75VDC Vin --> LM5009 buck (output 14V) --> LDO TPS70933 (output 3.3V)
2) LM5009's load are feedback resistor (47K+10K) and LDO (3~4mA).
Issue Description
Step 1: When 75VDC Vin switches off, LM5009's output 14VDC signal s dropping slowly due to the load is light.
Step 2: When LM5009's output 14VDC signal is dropping at 2.5VDC, 75VDC Vin switches on again, LM5009 can't rebootstrap due to LM5009's output 14VDC signal is not zero.
Finally, LM5009's bootstrap pin keeps as 6.5VDC and LM5009's output 14VDC signal keeps as 2.5VDC steadily.
My question:
1) Even if LM5009 is at the Gate drive UVLO status, there is still a small current goes to load ? If yes, how much of this leakage current or discharge current ?