Other Parts Discussed in Thread: LP8758
Hi,
I had used TPS65266RHBR in my previous design of board. But there is slight change in the design and I am looking for a new PMIC with below requirements:
Vin(typical)= 3.3V
Vout 1: 1.1V
Iout1: 3 to 4A
Vout2: 1.8V
Iout2= 2A to 2.5A
Vout3(Load switch preferably): 3.3V
Iout3: 1A
Kindly suggest me a PMIC