Hello,
My customer encountered an issue which the level of the overvoltage protection was not constant.
When VREF is 0.6V, they consider that the level of the OVP is max 1.05V VOUT according to the table below.
If VOUT = 1.05V, then about 0.729 will be input to the RSP pin.
However, OVP works when the actual VOUT is 1.1V to 1.13V.
Please advise on the cause of this symptom.
Thank you.
JH