This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2412: High Voltage Application

Part Number: TPS2412
Other Parts Discussed in Thread: UCC29002,

 Hi,

I am designing a power supply module with universal- AC input and 100W,35V output. I have a paralleling requirement  for this AC-DC power supply, which means if needed user can parallel these 2 to 3 modules together to increase the overall power output or to increase the reliability of the power supply modules.

but i also have a hotswapping requirement for N+1 modules parallel redundancy solution. for this requirement  I could see  UCC29002+TPS2412 ic combination to achieve the parallel and redundancy solution.

since my output bus voltage is 35VDC, i can UCC29002 for this voltage level, but  for TPS2412 in datasheet it is mentioned to use Controls Buses From 0.8 V to 16.5 VDC only.

how can I use this TPS2412 ORing power rail controller for this 35VDC bus voltage? is there any reference design for this voltage level for tps2412?

Thanks.