Part Number: BQ24075T
Other Parts Discussed in Thread: BQ24074
Hi,
Looking at the datasheet, in order to use BQ24075T on an existing design for BQ24074, I need to:
- Replace the ITERM resistor with a zero ohm resistor to tie SYSOFF to GND to enable it.
- Reduce input voltage to maximum 6V.
I think that is all to make it to work?
Due to BQ24074 shortage, I think this is the only way.