This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563201: TPS563201 maximum load capacitance

Part Number: TPS563201
Other Parts Discussed in Thread: TPS563202

 I was targeting to use TPS563201DDCR, but I noticed is maximum load capacitance for stability was only 68UF for the tightly coupled capacitance (LC filter). I am concerned because other parts of my board would add capacitance that would exceed the 68uF limit.

I was planning to have additional capacitance on the targeted 5V rail a little bit away from the LC section. My understanding that other capacitance does not necessarily get factored into the LC limitation for stability. However, what I don't understand is how I define how far away my other capacitance would need to be for it not to affect the stability.

Also is there a new maximum capacitance that the part would then be stable to. For example could I have 150uF capacitance total on the rail.

 

There is the TPS563202 which seems to have double that capacitance but I am having a hard time telling the differences between these parts or if there is a better part for a 5V 3A supply for an input up to 14V