This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650250: LDO unused pin

Part Number: TPS650250

Hi team,

I have checked below the process when the LDO output is not used, what capacitance does the small ceramic capacitor refer to?
What is the recommended capacitor size?

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/339455/tps650250-unused-ldo?tisearch=e2e-sitesearch&keymatch=TPS650250%252525252520unused#

Sincerely.
Ryu

  • Hello Ruy,

    I have assigned this to product expert. Please expect answer by tomorrow. 

    Datasheet specification seems to indicate minimum capacitance of 2.2uF, so at least with that value the LDO is proven and tested to be stable and not trigger false faults etc. I'll let Brenda to elaborate if she knows the minimum value in no load condition.

    Thanks.

    Regards,

    Tomi Koskela

  • Hi Ryu,

    You can use the minimum output capacitance in the spec for the unused LDO. I recommend using 2.2uF as Tomi recommended to make the rail is stable and doesn't trigger any false faults. 

    Thanks,

    Brenda

  • Hi Brenda and tomi,

    Thanks for the reply.
    I understand that 2.2μF is recommended.
    I think it should be as small as possible, but up to how much is acceptable to connect?

    Sincerely.
    Ryu

  • Hi Ryu,

    2.2uF would be our recommendation as it is the capacitance value we have validated across temperature for the stability of the LDO. 

    Thanks,

    Brenda

  • Hi Brenda,

    Thanks for the reply.
    I understood it well.
    Sorry for asking so many questions.
    I would like to know the maximum possible connection.

    Sincerely.
    Ryu

  • Hi Ryu,

    What do you mean by "maximum possible connection"? What are you referring to? 

    Thanks,

    Brenda

  • Hi Brenda,

    The maximum capacitance of the capacitor to be connected.
    I would like to check how much larger capacitor than 2.2μF can be connected.

    Sincerely.
    Ryu

  • Hi Ryu,

    In the TPS650250 spec we only specify the minimum capacitance required for the stability of the LDO. This device has an evaluation module (TPS650250EVM-447) that can be used to evaluate the PMIC performance under different conditions. Output voltages as well as external passive components like output caps can be changed as needed to match specific application use cases. 

    Thanks,

    Brenda

  • Hi Brenda,

    What I am asking is the capacitance of the capacitor when the LDO is not used.
    I would like to know the maximum value that can be connected in this case.
    Because the answers in other threads stated that it should be as small as possible.

    Sincerely.
    Ryu

  • Hi Ryu,

    Even though your application will not be using one of the LDOs, the minimum output capacitance (2.2uF) is still required for the unused LDO because both regulators share the same enable signal. For the unused LDO, the critical parameter would be the minimum capacitance for stability which is the 2.2uF we specify in our datasheet. The maximum capacitance for an unused rail should not be a concern because there wont be any load connected to the output so you just need the minimum capacitance to keep the overall power area small. Could you please share more information on your concern related to the maximum capacitance for the unused LDO? 

    Thanks,

    Brenda

  • Hi Brenda,

    Thanks for the reply.
    I understand now.
    I asked because it said that I need to connect as small a capacitance as possible.
    For example, if I don't have a 2.2μF capacitor, can I connect a 10μF capacitor?

    Sincerely.
    Ryu

  • Hi Ruy,

    In the other thread it was mentioned to use a small ceramic capacitor for the unused output. Small was just indication of low cost/small board area etc. because it is not critical for performance. It did not say as small as possible. As long as the value is 2.2uF or higher you are fine.

    Thanks.

    Regards,

    Tomi Koskela

  • Hi Tomi,

    Thanks for the reply.
    I understand.

    Sincerely.
    Ryu