This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25069: Design review

Part Number: LM25069
Other Parts Discussed in Thread: TPS2595, TPS2597

Hi Team,

Our customer is using the LM25069 in their board and would like to ask for a review. Kindly refer to the details below:

For Vsys=12V, I will put that hot-swap controller in the Master board 12v 5A, and that controller is used before the connectors go to 2 slaves connectors 12v@2A Each, so this is my design, Can you also advise me with an N channel MOSFET to use in this application.

Thanks in advance.

Regards,

Marvin