Hello everyone,
I would want to know the maximum admissible voltage on IADJ pin. Indeed, the datasheet only indicates that voltage on IADJ pin is clamped by an internal 1.24V zener (see figure 20), so what would happen if a superior voltage is applied (eg 5V)?
In absolute maximum rating, it is indicated that maximum current on IADJ is +/5 mA.
So, my first reflex would be to simulate with PSpice and find the voltage that would induce 5mA current in IADJ pin.
Am I correct ?
Thanks a lot in advance.