Part Number: BQ24160
Other Parts Discussed in Thread: BQ500212A
When using the IN source I see faults at just below 4.1V. About 75% capacity. My charge current is 300mA. It will charge for some number of seconds(3-20) then fault and repeat. The net effect is a very slow charge. If I drop the charge current to anything lower the process is similar but the charge/discharge ratio is fairly even and it just hovers at 75% capacity. When I use the USB source my current is above 500mA and charging appears just fine.
I'm unclear why it faults on the IN source. When the battery is below the 75% threshold I can drop the current as long as I stay above the 75mA threshold mentioned as the current sink for the IN source. Charging works normally until I hit just below 4.1V. It seems close to the DPPM threshold of 4.2 so I suspect that is related but I'm not sure.
Even when I have a >300mA IN source why does the current drop so much to cause continuous faults?