Hi team,
customer want qualify our TLV75509 as 2sd,
1. can we keep these FB resistor since we're NC , no affect right?
2.and what's the meaning of that PR5154 ? is that necessary?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
customer want qualify our TLV75509 as 2sd,
1. can we keep these FB resistor since we're NC , no affect right?
2.and what's the meaning of that PR5154 ? is that necessary?
Hi Fred,
I apologize for the delayed response.
There is no internal connection for Pin 4. However, be aware that leaving the resistors will load the LDO to ~57uA.
This device has an internal Pull-Down resistor for the EN pin, therefore no need for PR5154. Often times, there is no internal pulldown, and an external one is used.
Best,
Edgar Acosta
I see ,
but it won't be a big deal if we keep the PR5154 right?
since I don't know if RT9078 has this internal pull-down function
Hi Fred,
There is no issue keeping PR5154, the internal pull-down resistor is 120-Ω from EN to GND.
Best,
Edgar Acosta