Other Parts Discussed in Thread: TPS92638-Q1, TPS92633-Q1
Parça Numarası: TPS92638-Q1
Preliminary information
My IC (TPS92638QPWPRQ1) supply voltage will be 28V (Vsupply: 28V)
The MCU I use is powered by 5V.
I'm thinking of pulling the fault pin to pull-up externally with 5V, but I have some concerns (picture-1)
Fault pin internal structure; The fault pin seems to be pulled-up internally with Vsupply (picture-2)
Question1-) Is the connection type shown in picture-1 correct?
Question2-) Is there a possibility that the fault pin will give voltage higher than 5V and corrupt the MCU? (pic-1 // While Vssupply assuming 28V)
picture-1

picture-2