This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110EVM-796: For Lead Acid Battery.

Part Number: BQ34110EVM-796


Hi Ti

I am using bq34110EVM-796 Evaluation Module connected as below.

Using this for Lead Acid Battery. (12V@ 12AH).

Below is the problem 

All of sudden Time to empty went to 3 mins,

  

Before at 13:12(time) it was showing 48 mins to empty

But At 13:21(time) TTE its showing as 3 mins

could you pls say why it happened (and i had set EDV_CMP and Fixed_EDV0 Bits are set High , and Fixed EDV0 is set to 1755) 

Attaching the log data

.New_Battery1_Discharge_Profile.log

Also Ima attaching the gg file for reference.

gg file for pb Bat 09-06-2022.gg.gg.csv