Hello Team,
I have a few technical questions regarding the TPS389006-Q1, which I was not able to figure out with the preliminary dataheet.
In table 12-1 and -2 of the datasheet, I found some information regarding the under and over voltage threshold of the device. Does it mean, that the preliminary (pre-production) IC can only monitor voltages from 0.2-1.745V?
In our application we would need at least up to 3.3V.
Furthermore I have seen that the device is able to work with 1.8V and 3.3V interfaces. How to set this configuration? How to set DEV_CONFIG.SOC_IF1?
Is it right that you will offer different devices and the pre-production device features only 3.3V.
Can you give me some information about the timeline, when can you offer the mass production devices with 1.8V interface voltage?
Best regards,
Fabian