Other Parts Discussed in Thread: TINA-TI
Hello,
I am using this to drive a SiC mosfet and the simulation is being done on TINA-TI, but I am not getting anything at the output that looks like a pulse.
Note: This is PWM_LO_1
I do not understand why I have to set the DC level (V) at 5V. If I do not have TINA, TI can not simulate the circuit for me.
I get this error when I set DC Level (V) to 0V
I should be able to probe the output and see the expected pulse, but it does not at all give me a DC voltage of 15V.
I need help with the IC and also simulation.
Regards,