Other Parts Discussed in Thread: TPS62097
Hi Team,
My customer wants to know is it safe to apply 5V constantly on output side when there is no voltage applied on input side, could you kindly help confirm? Thanks.
Regards,
Jo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jo,
Mostly yes as this just turns on the HSFET body diode and results in a voltage Vout minus the diode drop at Vin. You need to check for any reverse current levels and ensure voltage ratings are not violated which does not seem to be an issue here with 5V. I recommend checking all 7 points listed in this app note: https://www.ti.com/lit/an/slyt689/slyt689.pdf
Thanks,
Amod
Hi Amod,
Thank you.
Customer wants to know following, could you kindly help?
1. The value of HSFET body diode voltage drop
2. reverse current rating.
From the material you shared, it says following. And TPS54228 have 2Amax Operating output current, so the reverse current rating will also be 2A?
"Since the input supply rail is powered from the output, there is reverse current flow through the IC to the other circuits on the input rail. The average reverse current should be kept less than the forward current rating of the IC. For example, the TPS62097 general-purpose industrial IC has a 2-A rated current. "
Thanks.
Regards,
Jo
Hi Jo,
Yes the reverse current rating can be limited to 2A. The HSFET body diode drop isn’t characterized but should be in the 0.6-0.7V vicinity. Best option is to check the drop on an EVM or any test board at the reverse current you expect to flow.
Thanks,
Amod