This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27520-G4: changing BATLSPUEN from high to low - impact on other bits

Part Number: BQ27520-G4

0520_3_29-bq27520G4_10.txt0520_3_29-bq27520G4_GF11.2.bq.fs.txt

I want to make a single bit change (BATLSPUEN from high to low) to an existing golden file and noticed that a bunch of  other bits change as well. I'm concerned that this single bit change messes up other bits and therefore the new golden file is not usable anymore.

Can you explain what other bits are changing? Or is it just checksums that we don’t have to worry about?

Original golden file: 0520_3_29-bq27520G4_10.bq.fs

Modified golden file: 0520_3_29-bq27520G4_GF11.2.bq.fs