I was trying to check whether the gauge is learning in the field?
I charged and discharged a single battery several times to see how the gauge is updating Qmax and Ra-tables. Prior to that I programmed the golden file.
I noticed that only the 'Cycle Count 0' updates but no other parameter.
Is the gauge still learning or is learning somehow disabled? I suspect that maybe my golden file set the Ra Status and Ra Flag to the incorrect values:
Ra0 Default: Status = 00, Flag = 55
Ra1 Default: Status = 00, Flag = 55
Ra0: Status = 00, Flag = 00
Ra1: Status = 00, Flag = 55
Ra0x Default: Status = 00, Flag = 55
Ra1x Default: Status = 00, Flag = 55
Do those Stati and Flags look ok? If yes, what else could cause the gauge not to learn in the field?
Thanks.