This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMS1587: Dimensions or tolerances

Part Number: LMS1587

Hi Team,

Our customer would like to request some mechanical dimensions of LMS1587ISX-3.3/NOPB which are not included in the datasheet.

He is looking for the following information:

The bottom side of package  please provide dimension of the body /  assembly outline since it only has the 0.200 in   / 5.08 mm min.

For the leads (side view) please your support with the max & min dimensions specific for:

MIN & MAX lead dimension 1.98 mm / .078 inch

MIN dimension for :  14.35  mm / 0.565 inch since this is the max

MIN dimension for lead : 1.27 mm / 0.050 inch since this is the max. 

Attached is the screenshot of the device and the dimensions that he is looking for.

TI questions .docx

Regards,

Danilo