This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24105: BQ24105 chip to run at 86 degree

Part Number: BQ24105


Hi Team

Our customer have a MeanWell AC-DC power converter running 15V 20W 1.4A running into a board built to TI specs. Charging a 3 cell Li-ion battery pack, the cells are 16850 type. The customer that built it wanted it to charge in under 3 hours. The question is what would cause the converter and the BQ24105 chip to run at 86 degrees C?

I hope you can help.

Regards,

Marvin