Hi
I am using the LM2736XMK/NOPB to convert 15V to 6V but unfortunately below design is not regulating the output and I can not figure out what is going on.



I even try to simulate using Web Bench and I am getting correct voltage.
As I increase the input voltage the output is changing too. Can you take look at my schematic and see if you find issue.
L= 6.8uH NLCV32T-6R8M-EFR
Cout = Cin = 10uF
Diodes: D11=D12 PMEG3005EH,115
Cboost = 10nF
Let me know if you want me get some graph from output.
Thanks