This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
In Figure 9 of SNVA097B you showed the Application Circuit. We understood most of it, but not the Function of D7 in the feedback path.
Best Regards Rolf
Hello Rolf,
I need to know the part number of the schottky diode you used to replace D7.
Also, what is the typical voltage at +SB / TP4 when operating normally?
Thanks,
Eric
Hi Eric
We are using dfls1100q-7. Can't tell /measure the voltage on T4, the board is in a case.
What's the purpose of D7?
Best Regards
Rolf
Hi Rolf,
I was double-checking with my colleague before describing the functionality of D7. We believe this diode clamps the reference to U3B-5 during startup (i.e. +SB is very low) and provides a bit of a soft start function before U4 (1.2V reference) is fully on.
Can you remove D7 and test/compare startup waveform?
A schottky diode has a relatively high leakage, especially when it is hot. If D7 has significant leakage it will raise the reference to U3B-5 via R33 (20k). I think this explains why your output voltage starts increasing after a few minutes.
Regards,
Eric
Hello again Rolf,
There is another possibility for D7. When the system shuts down and SB+ becomes 0V, D7 will discharge capacitor C30 very quickly. C30 is located at U3B-5, the reference for the control amplifier. Discharging C30 quickly sets the system for a quick restart. Without D7, C30 must discharge through R33 and R34 (30k), forming a time constant of 3ms.
Regards,
Eric