Hello team,
How BQ24616 behave when undercurrent condition at the input side?
For example, I_charge is set by 1A and then if adapter provide only 0.5A, how does it operate?
Best Regards,
Austin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
How BQ24616 behave when undercurrent condition at the input side?
For example, I_charge is set by 1A and then if adapter provide only 0.5A, how does it operate?
Best Regards,
Austin
Hello Austin,
It all depends on your input voltage and battery voltage. As this is a buck charge controller, your final battery voltage has to be less than your input voltage. As such, any step down in voltage is likewise a step up in charge current to maintain the power balance.
However, you also have a system load directly connected to the input in charging. You need to make sure that the total output power (charge current x charge voltage + load current x load voltage) does not exceed the input power. You can take advantage of using IINDPM, which will place a limit on the input current drawn from the adapter by reducing the charge current as necessary. There is no limit on the input voltage however, and if you overdraw the adapter before you hit IINPDM the input voltage will start to collapse.
Regards,
Mike Emanuel
Hi Michael,
Thanks for reply.
The customer has more detailed question.
Output voltage and current are set by 13V / 1A and then if Adapter provide only 15V / 0.5A(current is limited by any reason), how BQ24616 operate?
Best Regards,
Austin
Hi Austin,
Here you are requesting 13 W of output power with 7.5 W of input power at the max charge voltage. At the max charge voltage you cannot supply enough power. If your IINPDM is not set to 0.5 A appropriately your input will start to drop. If your IINPDM is set to 0.5 A you will charge the battery with 7.5 W of input power, lowering the charge current as necessary to achieve the power balance.
Even at the LOWV threshold of 1.55 VFB or 9.6 V Battery you will still be able to supply enough power to charge the battery at 1 A.
Please make sure you have enough power to charge the battery without overloading the supply and make sure you limit the input current according to the adapter limits.
Regards,
Mike Emanuel