Other Parts Discussed in Thread: TPS53219A
What is the difference between TPS53119RGTR & TPS53219ARGTR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thanks for reaching out. I will look into this and respond to you soon.
Best,
Calan
Hello,
The main difference between these two devices is that TPS53119RGTR has Input voltage range: 3v to 26v while TPS53219ARGTR has Input voltage range: 3v to 28v.
In addition, TPS53119 is slightly more expensive than TPS53219A.
Under section 6.1 of the datasheets of both devices titled "Absolute Maximum ratings", there are differences in the stress ratings:
TPS53119 VDD: -0.3 to 26v. DRVH: -2 to 35v
TPS53219A VDD: -0.3 to 28v DRVH: -2 to 37v
Also, TPS53219A has Wide output load range: 0 A to > 20 A
Best,
Calan