This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62932: TPS62932 setup as inverting converter

Part Number: TPS62932
Other Parts Discussed in Thread: TPS62933

Hi

I am designing in the TPS62932 into a new product. We need 4 of them in each product and maybe 5 if it works well as an inverting converter.

We have 16-22V Input and need to get -15V at 0.5A output.

Do you have any schematics where the  TPS62932 or TPS62933 is used as inverting converter?

The other power rails are straight forward and I already designed them with the TPS62932.