Part Number: LM336-5.0
Texas Instruments
Dear person in charge
Hello,
Thank you for your continued support.
My name is Kengo Suzuki from Daifuku.
Case Number: CS1162154
I would like to ask your company again about the measurement method: 5V Reference Diode (aka Zener Diode): LM336MX-5.0/NOPB with HP 34401A digital multimeter, the maximum measurement speed is 1000 times/sec (= 1msec sampling).
What is the basis for your company's measurement of the 5V reference diode: LM336MX-5.0/NOPB using this instrument with a maximum measurement speed of 1000 times/sec (=1msec sampling)?
The board on which our LM336MX-5.0/NOPB is mounted is used for a current input/output circuit that samples at 0.1msec (=100μsec).
I would like to measure the current with 0.01msec (=10μsec) sampling, but even the successor to the measuring device you introduced, the 34461A (Keysight Technology), can only measure up to 1000 times/sec (=1msec sampling).
I am sorry to trouble your company and would appreciate it if you could enlighten me.
Best,
Kengo