This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: About setting of Sink PDO

Guru 21045 points
Part Number: TPS25750
Other Parts Discussed in Thread: USB-PD-CHG-EVM-01, , BQ25792

Hi Team,

 

Currently, our customer are evaluating the following conditions.

Source: 45W PD adapter

Sink: USB-PD-CHG-EVM-01

Tool: Advance configuration of Application_Customization_Tool ver7.0.3

 

They would like to set 20V/2.25A so know the proper Sink PDO setting.

I understand the following setting.

Is my understanding correct?

 

[Our settings]

Sink PDO1 15W (5V*3A)

Sink PDO2 27W (9V*3A)

Sink PDO3 45W (20V*2.25A)

 

[PDO3 setting picture]

 

Regards,

Hide