Other Parts Discussed in Thread: CSD18563Q5A, LM25145
Hi,
I am uisng LM3150, so far it is good. But I am curious one thing for chip temperature.
Test setting is: 24V input, wihout loading, with the different output voltage.
The question is that, why the chip temperature is so higher with over 10V and without loading? With higher output voltage, and the chip temperaure increase too much?
Best Regards,
Kent