I am using a LM27341MY/NOPB in a design to take a 12V input to +5V out.
The output seems to be inconsistent (seems related to start up), its very inconsistent but I would say 1/5 power ups the output goes to +5V as expected. The other 4 times it will have a steady state output of approximately 0.7V. I have attached two captures that illustrate the "expected" startup and a capture in which it does not start up properly. I have also attached a snippet of my schematic.
Any help would help, thanks.