This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27341: Inconsistent Startup Behavior

Part Number: LM27341

I am using a LM27341MY/NOPB in a design to take a 12V input to +5V out.  

The output seems to be inconsistent (seems related to start up), its very inconsistent but I would say 1/5 power ups the output goes to +5V as expected.  The other 4 times it will have a steady state output of approximately 0.7V.  I have attached two captures that illustrate the "expected" startup and a capture in which it does not start up properly.  I have also attached a snippet of my schematic.

Any help would help, thanks.