The line regulation of the LM3671 claims to be 0.031% while the closest alternate that I can find in the same package size is about 0.26%. There is a large difference between the two according to the datasheets but I need to know if this claim is accurate or a typo. Something doesn't seem right with it. What alternatives exist that are comparable in a SOT-23-5 package?