Other Parts Discussed in Thread: TMS320DM8168
Hi All,
We are using TPS40400 in our design for supplying AVS core supply to TMS320DM8168 processor. The address of the TPS40400 is programmed to 0x38(70 in octal) using resistors. The TPS40400 is connected to TMS processor through I2c. When we run I2C probe command for listing the connected devices in the Bus, we are getting acknowledgement at 0x0C along with the slave devices connected to the I2c bus (Including 0x38). There is no slave with address 0x0c in our device. We found TPS40400 acknowledging for 0x0C. This will happen only one time even if we do I2c probe multiple times, can anybody explain this? .
Below I am attaching the images captured when device acknowledge at 0C with data 0x70.
when we disconnect Tps40400 from bus negative ack only getting for 0x0c