Hi,
We test the TPS40057 for our new design and the Inductance scream when the power on( the light also has the inductance scream), when we load the increase circuit load, the scream is more intense,
Pleaes kindly review the below circuit and advies how to solve this issue? thanks.
The parameter as below: Input voltage: 24VDC, output voltage: 4.3VDC, max. current: 20A, Inductance: 4.7uH, Fsw=300KHz;
Schemtic diagram as below: